View a function reference
Once it has been added, a function may be referenced multiple times within a library object. Functions added to a project or controller library object may be referenced from within multiple library objects.
These are examples of ways a function can be referenced:
- As a field value for a parameter or library object elements
- As part of an expression
- As part of a substitution
- As part of another function
To view a function reference
- In theLibrary Objectspane, click the library object that contains the function of interest.
- In the decorator pane, on theFunctionstab, right-click the function and then clickShow References. The References window opens. ClickNavigatefor the reference listing. The decorator panel opens for that element.
- ClickOKto close theReferenceswindow.TIP:To access the fields in the decorator panel, theReferenceswindow must be closed.
Provide Feedback