Configure an element substitution
Element substitutions are performed to replace an element during instantiation. Elements that can be substituted include modules, tasks, programs, and routines.
To configure an element substitution
- In theLibrary Objectspane, expand the library object folder that contains the element to be substituted.
- Click the element, the decorator pane displays the element attributes.
- Next to an attribute for which to substitute a different value (such as Name, Description, or ParentModule) click the ellipsis (...) button to open the Substitution Builder window.
- Configure the substitution as needed.
- ClickOKto save the substitution.
Provide Feedback