Import library object members
Import all or selected Functions, External References, Linked Libraries and Interfaces to transfer them from another system, library, or a backup. The Import functionality uses a previously created Export file and is applied to individual libraries. Library object parameters must be imported separately.
To import library object members
- InLibrary Objects, right-click an individual library.
- In the right-click menu, selectImport Members.
- Browse to and select an export file, then selectOpen. Import Members appears in the center ofLibrary Designer.
- InImport Members, select an Action for each member or dependency.The default Action is determined based on the content in the destination library. Dependencies are not automatically included or excluded based on member Actions and must be selected individually.
- SelectImport.
- Review the validation results, then selectContinue.
Provide Feedback