Import Members
How do I open Import Members?
- InLibrary Objects, right-click an individual library.
- In the right-click menu, selectImport Members.
Use
Import Members
to select Functions, External References, Linked Libraries, and Interfaces to import from another system, library, or backup.Column | Description |
|---|---|
Name | Displays the name of the item, grouped into Functions, External References, Interfaces, or Linked Libraries. |
Action | Selects an action to perform during import. Available actions vary based on the destination library:
The default Action is determined based on the content in the destination library. |
Type | Displays the type of the item. |
Source Library | Displays the name of the source library or library scope. |
Details | Opens a read-only editor panel to display specific associations for the item. |
Depends On | Lists associated dependencies of the item. |
Used By | Lists associated members of the item. |
Description | Displays the description of the item. |
Provide Feedback