Export library object members
Export all or selected Functions, External References, Linked Libraries and Interfaces in a library definition to transfer them to another system, library, or backup. The Export functionality is applicable to individual libraries where each library can be exported into a separate file. Library object parameters must be exported separately.
To export library object members
- InLibrary Objects, either:
- Right-click an individual library.
- Right-click an individual member such as a Function.
- In the right-click menu, select Export Members.Export Membersappears in the center ofLibrary Designer.
- InExport Members, select or deselect members to export.By default all members and dependencies are selected. Dependencies are included or excluded based on member selections.
- SelectExport, then selectSave.
Provide Feedback