Export Members
How do I open Export Members?
- InLibrary Objects, either:
- Right-click an individual library.
- Right-click an individual member such as a Function.
- In the right-click menu, selectExport Members.Export Membersappears in the center ofLibrary Designer.
Use
Export Members
to select Functions, External References, Linked Libraries, and
Interfaces to back up or transfer to another system or library.Column | Description |
|---|---|
Name | Displays the name of the item, grouped into Functions, External References, Interfaces, or Linked Libraries. |
Export | Selects a member and its dependencies for export. |
Type | Displays the type of the item. |
Source Library | Displays the name of the source library or library scope. |
Details | Opens a read-only decorator panel to display specific associations for the item. |
Depends On | Lists associated dependencies of the item. |
Used By | Lists associated members of the item. |
Description | Displays the description of the item. |
Provide Feedback