Add a service
- In the, access the section.FactoryTalk® Remote Access™Manager
- In the domain (left) pane, select the subdevice.
- In theServicepane on the right, click thecircled plusbutton.
- ACreate servicedialog window opens. Complete all the required fields:
- Name: The subdevice name. Unless renamed by the user, it is equal to theService type.
- Service type:
- Custom: Executes an application by using a command line that you enter in theCustom actiontext box.NOTE: See Custom service application example to view theSSH via PuTTYapplication example.NOTE: If theService typeis set toCustom, thePortandPathsettings are not available.
- RDP: (Remote Desktop Protocol) Opens a Microsoft RDP client to the specified IP.
- HTTP: Opens a new browsing window to the specified IP.
- HTTPS: Opens a new browsing window to the specified IP.
- VNC: Provides remote desktop access to subdevices equipped with VNC servers. See VNC connection to subdevices.
- Port: The subdevice port through which the communication is established.NOTE: This setting is available if theService typeis set to theRDP,HTTPorHTTPSservices.
- Path: The URL path of the web service.NOTE: This setting is available only if theService typeis set to theHTTPorHTTPSservices.
Once you created a service, you can launch it. See Launch a service.
Provide Feedback