Entitlements

Two entitlement types are available for
FactoryTalk® Remote Access
: domain and Runtime entitlements.
NOTE:
See How to activate a entitlement to learn how to activate an entitlement.
See Entitlements in the
FactoryTalk® Hub
online manual for further information on entitlement purchasing and allocation.

Entitlement types and upgrades

  • FactoryTalk® Remote Access
    Runtime entitlements:
    Allows HMIs or IPCs to connect to
    FactoryTalk® Remote Access
    and determine the operations that are granted by that connection. Devices are provided by default with a Runtime entitlement that may consist of a
    Pro
    or
    Basic
    entitlement.
    The Pro entitlement upgrade allows yout to obtain extra features. This means that the Basic entitlement remains assigned to the device and you cannot rehost the Basic entitlement to other devices.
    NOTE: To learn more about what license is assigned to each device by default, see the device sections listed under System components.
    To upgrade a Basic entitlement, you can purchase a
    Runtime Upgrade
    entitlement, which transitions the entitlement from Basic to Pro. If you already possess a Pro entitlement, you can elevate your Basic entitlement by selecting the existing Pro entitlement during the upgrade process.
    To upgrade your entitlement, proceed as follows:
    1. If you do not have any existing Pro entitlement, purchase an
      Upgrade from Basic to Pro
      entitlement on the Commerce Portal for your organization. The purchased entitlement is then visible on
      FactoryTalk® Hub
      .
      NOTE: Refer to the
      FactoryTalk® Hub
      online manual
      for further information on how to manage your entitlments.
    2. In
      FactoryTalk® Remote Access
      , go to the
      Domain view
      section.
    3. Select the device for which you want to upgrade your entitlement.
    4. In the right pane, under
      Entitlements
      , select
      Upgrade
      .
    5. Select the
      Runtime Upgrade
      entitlement you previously purchased that is now visible in FactoryTalk Remote Access, or choose an existing Pro entitlement.
    NOTE:
    • If you want to detach a Basic entitlement, you must first detach any Pro entitlement upgrades, if present.
    • If you remove a device from a domain, any entitlements assigned to it become available for rehosting.
    See the table below for further information about the Basic and Pro entitlements:
    Entitlement
    Description
    FactoryTalk® Remote Access
    Runtime Basic
    Basic entitlements allow file transfers, task management, and minimal VPN capabilities.
    NOTE: OptixPanel Compact graphic terminals display an
    Upgrade
    button next to the Basic entitlement type, in the right pane of the
    Domain view
    , in the Entitlements section. This button allows you to upgrade the Basic entitlement to the Pro entitlement by purchasing just the services that are not already included in the Basic entitlement.
    FactoryTalk® Remote Access
    Runtime Pro
    Pro entitlements allow VPN access to all devices on the device network, file transfers and task management.
  • FactoryTalk® Remote Access
    1/2/5/10/25/50 Concurrent Connections entitlements:
    This domain entitlement may be purchased in volumes of 1/2/5/10/25/50 concurrent device connections.
  • FactoryTalk® Remote Access
    Trial Bundle:
    This entitlements bundle includes a domain entitlement for concurrent connections and four Runtime entitlements. It consists of a temporary entitlements bundle including:
    • FactoryTalk® Remote Access
      2 Concurrent Connections entitlement*
    • Two
      FactoryTalk® Remote Access
      Runtime Basic entitlements
    • Two
      FactoryTalk® Remote Access
      Runtime Pro entitlements
    *Once the Trial Bundle is activated by your Sales Representative, you will find the newly assigned domain in
    FactoryTalk® Remote Access
    Manager.
    NOTE: See Trial Entitlements in the
    FactoryTalk® Hub
    manual for further information on this subject.

Entitlements expiration

When an entitlement expires, the domain connected to it expires too.
  • FactoryTalk® Remote Access
    Runtime entitlements
    are perpetual, including Runtime entitlement upgrades.
  • FactoryTalk® Remote Access
    1/2/5/10/25/50 Concurrent Connection entitlements
    expire after 365 days and a 7-days grace period following the expiration date activates to allow for entitlement renewal through the
    FactoryTalk® Hub
    . If the entitlement is not renewed within the grace period, the user can still access the domain, without being able to carry out any action within it.
    Select the
    Settings
    Domain options
    Send e-mail notifications of account information
    entry to allow each admin and owner user to receive an email every day during the grace period, informing them about any days left to the entitlement expiration.
    NOTE: 60, 30, and 10 days before the
    FactoryTalk® Remote Access
    1/2/5/10/25/50 Concurrent Connection entitlement
    expires, an email is sent to all of the admin and owner users to inform them about the expiration deadline.
  • FactortyTalk Remote Access Runtime Trial Bundle:
    The Runtime entitlements included in the Trial Bundle expire when the
    FactoryTalk® Remote Access
    2 Concurrent Connections entitlement expires. After expiration, no grace period starts.
    NOTE: For details about your Trial Bundle subscription duration and expiration date, contact your Sales Representative.
    NOTE: Notification messages will appear each time you log on to the service informing you of the number of days remaining in the Trial Bundle entitlement. After the trial period is over, you will not be able to use the service until you obtain a subscription.
NOTE: You can register a device to a domain while the same device is registered to another domain.

See your entitlements in
FactoryTalk® Remote Access

  1. Access
    FactoryTalk® Remote Access
    Manager.
  2. In the
    Permissions/Information
    pane, open
    Entitlements
    . This section shows the entitlements for both domains and device Runtimes in your organization.
    NOTE: In this area, you can see how many entitlements have already been assigned and how many are still available to you.

See your entitlements in
FactoryTalk® Hub

  1. Access your organization in FactorytalkHub.com.
  2. Select .
  3. Select
    View Entitlements
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal