- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Network interface
Configure the WAN and LAN network interfaces
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
DHCP activated | DHCPClientEnabled | Obtain IP settings automatically using DHCP | |
IP address | IPAddress | IP address of the network | |
DNS 1 | DNS1 | Primary DNS address of the network | |
DNS 2 | DNS2 | Secondary DNS address of the network | |
Default gateway | DefaultGateway | IP address of the default network gateway |
Provide Feedback