Configure Virtual Meter
Perform the following steps to configure
Virtual meter
formula and tag mapping:- Click theConfigurationtab.Configure Virtual Meter

- ClickEditand clickVariable.Virtual Meter Dashboard

- TheVariable Configurationdialog is displayed. Provide aVariable Name.
- UnderSelect Metersection, expand the tree and select theResource meterwith sameResource Type,Measurement (Consumption/Demand), and under the sameSite/Area/Work Center.Variable Configuration Dialog

- ClickSubmit.Valid Formula

- Click the [
] icon to add another variable. Users can add up to 15 variables.NOTE:- If another variable is not added after the
icon, Invalid Formulais displayed. - SameResource metercannot be added twice for the sameVirtual meter.
- When more than two variables are added,Valid Formulais displayed.Virtual Meter Configuration (Continued)

- ClickSave.
- The user can edit/delete any variable and add a new variable.
IMPORTANT:
- Maximum of 15 variables can be added while configuring the formula for theVirtual meter.
- Maximum of 15 virtual meters can be added under anySite/Area/Work Center.
- To delete the variable, clickClear Configuration.
ATTENTION:
If you encounter errors while configuring a virtual meter, refer to the Datalink Configuration section.
Provide Feedback