Production Meter Dashboard

This dashboard provided the detailed production data. It helps track energy intensity within production processes, enabling managers to optimize production efficiency, reduce energy waste, and enhance overall productivity.
Click
Production meter
from the hierarchy list.
The following table provides the list of charts available by default in the dashboard:
Chart Types
S.No
Chart/Widget Type
Description
1
Total Production (Harmonized)
This chart shows the current range and past range, along with the last value and last updated time.
2
Production Data
The user can view the selected time period with the respective granularity on the X-axis and production data on the Y-axis. This chart shows the production data summary.
Refer to Dashboard Features section to manage the Production Meter dashboard.
Related Information
:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal