LDS Registered Status

Description
This value indicates the status of the
FactoryTalk Linx Gateway
's registration with the OPC Foundation Local Discovery Server (LDS).The OPC LDS is a separate service installed by the OPC UA server by default and will be running on the same computer. The counter can appear as two statuses:
  • “Yes” indicates that the FactoryTalk Linx Gateway is registered with the LDS.
  • “No” indicates that the FactoryTalk Linx Gateway is not registered with the LDS.
TIP:
To enable this function, in
FactoryTalk Linx Gateway Configuration
>
UA Server
, select
Register with Discovery Service
.
For the latest version of the OPC LDS, visit the OPC Foundation's download site https://opcfoundation.org/developer-tools/developer-kits-unified-architecture/local-discovery-server-lds/.
Find more information on OPC UA Discovery and Global Services, visit: https://opcfoundation.org/developer-tools/specifications-unified-architecture/part-12-discovery/.
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC UA Server
Value
  • Type: String
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC UA server.
  • Updates: This value is retrieved when the configuration changes in
    FactoryTalk Linx Gateway Configuration
    .
  • Reset: This value will be retrieved when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal