Activation
Description
FactoryTalk Linx Gateway
MQTT service obtains the FactoryTalk Linx Gateway
activation from FactoryTalk Activation Manager. This value indicates the type and tag count of the FactoryTalk Linx Gateway
activation in effect. If no activation is found, the value will show “Activation not found”.Activation | Type | Supported Tag Count |
|---|---|---|
LINXGW.PROFESSIONAL | FactoryTalk Linx Gateway Professional | 40,000 |
LINXGW.DISTRIBUTED | FactoryTalk Linx Gateway Distributed | 32,000 |
LINXGW.EXTENDED | FactoryTalk Linx Gateway Extended | 15,000 |
LINXGW.STANDARD | FactoryTalk Linx Gateway Standard | 5000 |
LINXGW.BASIC | FactoryTalk Linx Gateway Basic | 1000 |
GOLDMASTER | Gold Master | 40,000 |
For more information on the activation type, see .
FactoryTalk Linx Gateway
HelpLocation
- FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost >FactoryTalk Linx GatewayMQTT Server
Value
- Type: String
- Source: This value is generated by theFactoryTalk Linx GatewayMQTT service. See the “Type” column in the table above.
- Updates: This value is loaded when the service initially starts.
- Reset: This value resets when you reset the service or restart the computer.
Provide Feedback