Fault codes, reset bits, types, and descriptions

The table below lists information about the fault codes for the Multifunctional Access Box. Faults are cleared (unlatched or reset) when one of these reset bits is acknowledged:
  • GeneralFaultUnlatch - Unlatches faults related to the bus device interface
  • LockSequenceFaultUnlatch - Unlatches faults related to the locking sequence
    Fault codes
    Fault Code
    Fault Reset Bit
    Fault Type
    Description
    2721
    GeneralFaultUnlatch
    Emergency stop discrepancy time error
    Indicates the time between emergency stop Channel A and Channel B changing state exceeded the maximum allowable time (5 seconds).
    2722
    GeneralFaultUnlatch
    Enabling switch discrepancy time error
    Indicates the time between enabling switch Channel A and Channel B changing state exceeded the maximum allowable time (5 seconds).
    2723
    GeneralFaultUnlatch
    Door position discrepancy time error
    Indicates a discrepancy between both microprocessor channels of the device.
    2724
    GeneralFaultUnlatch
    Bolt position discrepancy time error
    Indicates a discrepancy between both microprocessor channels of the device.
    2725
    GeneralFaultUnlatch
    Guard locking discrepancy time error
    Indicates a discrepancy between both microprocessor channels of the device.
    2731
    GeneralFaultUnlatch
    Emergency stop test pulse error
    Indicates that no test pulses are being detected by the emergency stop monitoring circuit.
    2732
    GeneralFaultUnlatch
    Enabling switch test pulse error
    Indicates that no test pulses are being detected by the enabling switch monitoring circuit.
    2733
    GeneralFaultUnlatch
    Door position test pulse error
    Indicates that no test pulses are being detected by the guard door position monitoring circuit.
    2734
    GeneralFaultUnlatch
    Bolt position test pulse error
    Indicates that no test pulses are being detected by the bolt position monitoring circuit.
    2735
    GeneralFaultUnlatch
    Guard locking test pulse error
    Indicates that no test pulses are being detected by the guard lock monitoring circuit.
    2736
    GeneralFaultUnlatch
    Mode selector switch test pulse error
    Indicates failure of the mode selector switch. Check the signs of abuse and tampering. Turn the knob to change the switch position. Unlatch the fault by cycling output GeneralFaultUnlatch.
    2741
    None
    Maximum service life diagnostic message
    Indicates the device has reached the maximum mechanical lifetime (1,000,000 operations).
    2742
    None
    Internal device error
    Indicates an unrecoverable fault. The device may need to be replaced.
    2743
    LockSequenceFaultUnlatch
    Signal sequence error
    Indicates the device detected an unacceptable sequence of events (for example, guard locking is active while the guard door is in the open position).
    2744
    LockSequenceFaultUnlatch
    Lock device error
    Indicates the device detected activation of the escape release handle or the manual release.
    2745
    None
    Transponder read error
    Indicates an unrecoverable fault. The device may need to be replaced.
    2750
    None
    Power supply or parameter assignment error
    Indicates a problem with the power supply or a CIP safety parameter assignment.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal