Set Safety Network Number
- Choose the format for the safety network number:
- Time-based. The safety network number is generated based on the creation date and time (to the millisecond) of the device. If you choose this format, selectGenerateto generate the number.
- Manual. Enter a number from 1 through 9999, per network type. Once you have chosen your format, the safety network number appears in theNumberfield.
- SelectCopyto copy your safety network number to the clipboard.
- SelectOK.
Provide Feedback