Safety view

Use the
Safety
view to:
  • View or change the controller's safety level.
  • View the Safety application’s Lock and Unlocked status.
  • Change the Lock state of the Safety application.
  • View controller safety status information.
  • For controllers with SIL3/PLe safety level, view the status of the Safety Partner.
  • Generate and view Safety signature information.
  • Select whether the signature is protected from deletion while the Safety controller is in Run mode.
  • Select how the software handles the replacement of Safety I/O.
  • View or assign a unique safety network number to each port on the controller that supports a CIP Safety connection.
TIP:
When the Safety application is locked, you cannot generate a new Safety signature or delete an existing one.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal