Device definition dialog box

How do I open the Device definition dialog box?
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. In
    Devices
    , double-click the controller to open the device profile.
  3. In the device profile, select
    Device definition
    .
Use the
Device Definition
dialog box to:
  • View the device type.
  • Configure device-specific settings.
TIP:
The available parameters are based on the device being configured. Parameters that do not apply to the device are hidden.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal