Encoder Standard Configuration view parameters

The parameters on
Encoder Standard Configuration
define the standard connection to the controller.
Parameters
Parameter
Description
Monitor Input Voltage
Enable or disable voltage monitoring. Selecting this parameter enables voltage input monitoring.
Sync Standard Config to Safety
Sets the standard configuration parameters the same as the safety configuration: position scaling, resolution, revolutions, direction, velocity units, preset, endless shaft, numerator, and denominator. Standard configuration parameters are disabled and shown as blank when this parameter is selected.
Enable Position Scaling
Sets
Position Scaling
to 1 and enables the scaling function. For a single-turn device, Enable
Endless Shaft Functionality
is always disabled. In a multi-turn device, this parameter is only enabled when
Sync Standard Config to Safety
is cleared.
Enable Endless Shaft Functionality
Enables the endless shaft functionality. This parameter is only enabled when
Sync Standard Config to Safety
is cleared and
Enable Position Scaling
is selected.
Numerator
Sets the numerator for the endless shaft functionality, where the steps per revolution are set as a fraction. Valid values are from 1 through 4096. For a single-turn device, the value is hard-coded to 1. For a multi-turn device, the default value is 4096.
In a multi-turn device, this parameter is only enabled when
Sync Standard Config to Safety
is cleared and
Enable Endless Shaft Functionality
is selected. In a single-turn device, this parameter is never enabled.
Denominator
Sets the denominator for the endless shaft functionality, where the steps per revolution are set as a fraction. Valid values are from 1 through 65536. For a single-turn device, the value is hard-coded to 1. For a multi-turn device, the default value is 1.
In a multi-turn device, this parameter is only enabled when
Sync Standard Config to Safety
is cleared and
Enable Endless Shaft Functionality
is selected. In a single-turn device, this parameter is never enabled.
Resolution (CPR)
Sets the counts per turn. Valid values for
Resolution
are from 1 through 262144. When disabled, the value for
Resolution
is set to the default value of 262144. When
Enable Endless Shaft
is selected, the last value entered is displayed, but ignored.
This parameter is only enabled when
Enable Position Scaling
is selected and
Enable Endless Shaft Functionality
is not selected.
Revolutions
Sets the number of turns. For a multi-turn device, the valid values for
Revolutions
are 1, 2, 4, 8, 16, 32, 64, 128, 256, 512, 1024, 2048 and 4096. For a single-turn device, the
Revolutions
value is always disabled and hard-coded to 1. For a multi-turn device, the default value and the disabled value is 4096.
In a multi-turn device, this parameter is only enabled when
Enable Position Scaling
is selected and
Enable Endless Shaft Functionality
is not selected.
Range
When
Enable Position Scaling
is selected and
Enable Endless Shaft Functionality
is cleared, the value for
Range
is the
Resolution
value multiplied by the number of
Revolutions
. For multi-turn devices, the allowed values are 4 to 1073741824 and the default value is 1073741824. In a single-turn device, the allowed values are 4 to 262144, and the default value is 262144.
This parameter is only enabled for multi-turn devices when
Enable Position Scaling
is selected and
Enable Endless Shaft Functionality
is selected. If either
Enable Position Scaling
or
Enable Endless Shaft Functionality
is not selected, this parameter is disabled.
Direction
Set the
Direction
of the count to
Clockwise
or
Counterclockwise
. The default value is
Clockwise
.
This parameter is only enabled when
Sync Standard Config to Safety
is cleared.
Velocity Units
The default value is Counts/s. The valid values are:
  • Counts/s: 1F04H
  • Counts/ms: 1F05H
  • Revs/s: 1F0EH
  • Revs/min: 1F0FH
  • Revs/h: 1F10H
Configuring the velocity units also configures the acceleration units:
  • Counts/s -> Counts/s
    2
  • Counts/ms -> Counts/ms
    2
  • Revs/s -> Revs/s
    2
  • Revs/min -> Revs/s
    2
  • Revs/h -> Revs/s
    2
This parameter is only enabled when
Enable Position Scaling
is selected and
Enable Endless Shaft Functionality
is not selected.
Preset
Sets the
Preset
value, in counts. The maximum value is 1 less than the total measuring range. The valid values are 0 to (
Range
- 1).
This parameter is only enabled when
Sync Standard Config to Safety
is cleared.
Velocity number of pulses to average (Integration)
Sets the number of velocity values from which a moving average is formed. The valid values are from 0 through 128.
Velocity Filter Cutoff frequency (low pass bandwidth)
Sets the bandwidth of the low pass filter. The valid values are from 0 through 500.
Acceleration number of pulses to average (Integration)
Sets the number of acceleration values from which a moving average is formed. The valid values are from 0 through 128.
Acceleration Filter Cutoff frequency (low pass bandwidth)
Set the bandwidth of the low pass filter. The valid values are from 0 through 500.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal