Configure device window parameters
Configure device window parameters for the high-speed counter device.
To configure device window parameters
- On the tab for the device, selectWindows.
- In theWindowsview, fill in the parameters and selectOK.TIP:Use output tag members to configure parameters not editable in theWindowsview.
Provide Feedback