Windows view
Use the
Windows
view to:- View a summary of the device windows configured for the high-speed counter device.
- Configure which counter is associated with a window. The remaining parameters are not editable in theWindowsview, but are configurable using the device output tag members.TIP:Use theWindowsview inDevice definitionto define the mode in which a window operates when tied to a device counter.
Provide Feedback