Configure input parameters
Configure input parameters to define count direction and filter times.
To configure input parameters
- On the tab for the device, expandCounters, and then expand an individual counter.
- SelectInput.
- In theInputview, fill in the parameters and selectOK.TIP:Use members to configure parameters not editable in theInputview.
Provide Feedback