Device definition - Windows view parameters
The
Windows
view in Device definition
includes these parameters.Parameter | Description |
|---|---|
Window | Indicates the window to which this configuration applies. |
Mode | Defines the window mode. The windows activate the device's outputs. Available options are:
|
Provide Feedback