Device definition - Windows view
In
Device definition
, use the Windows
view to define the mode for each window. The windows can trigger output behavior so that the output responds to input conditions at high speed. The window Mode
determines the configuration parameters that are used with the window.
TIP:
- To configure windows parameters, setConnectioninDevice definitiontoData with EventsorData.
- These parameters are unavailable whenConnectioninDevice definitionis set toListen OnlyorListen Only with Events.
Provide Feedback