Device definition - Events view parameters
The
Events
view in Device definition
includes these parameters.Parameter | Description |
|---|---|
User Defined Data | Additional data to include when an event occurs. Define up to three user defined data instances per event. Available options are:
|
Provide Feedback