Device definition - Events view
In
Device definition
, use the Events
view to configure the user-defined data to include when an event occurs on the device.
TIP:
- To configure the events parameters, setConnectioninDevice definitiontoData with Events.
- The event parameters are unavailable whenConnectioninDevice definitionis set toListen OnlyorData.
- You must use aListen Only with Eventsconnection if the device is configured with aData with Eventsconnection. If you configure aListen Onlyconnection which doesn't support events and the device is configured with a Data with Events connection by another controller, the software may display the message:(Code 16#0108) Connection Request Error: Connection type (Multicast/Unicast) not supported.
Provide Feedback