Windows view parameters
The
Windows
view includes these parameters:Parameter | Description | Member Name | Value |
|---|---|---|---|
Counter | Determines the counter with which the window is associated. | C.Window0x.CounterSelect | 00 = Counter 00 01 = Counter 01 |
Output On Value | Shows the acceleration, count, frequency, or pulse width at which the Window turns on. | O.Window0x.On | -2147483648 to 2147483647 or 32-bit floating point value depending on configuration. For a window configured for frequency mode, this applies:
For a window configured for Pulse Width mode, this applies:
|
Output Off Value | Shows the acceleration, count, frequency, or pulse width at which the Window turns off. | O.Window0x.Off | -2147483648 to 2147483647 or 32-bit floating point value depending on configuration For a window configured for frequency mode, this applies:
For a window configured for Pulse Width mode, this applies:
|
Output On Hysteresis | Shows the negative offset from the Window.On value to apply hysteresis to. | O.Window0x.HysteresisOn | Any If the value <= 0, hysteresis is disabled. |
Output Off Hysteresis | Shows the negative offset from the Window.Off value to apply hysteresis to. | O.Window0x.HysteresisOff | Any If the value <= 0, hysteresis is disabled. |
Unit | Shows the unit for the individual window. | Not applicable | The Unit value is read-only and varies depending on the window mode defined in the Device definition dialog box.
|
Provide Feedback