Windows view

Use the
Windows
view to:
  • View a summary of the device windows configured for the 5069-HSC2XOB4 high-speed counter device.
  • Configure which counter is associated with a window.
    TIP:
    • To configure the remaining parameters in the
      Windows
      view, use the device output tag members.
    • To define the mode in which a window operates when tied to a device counter, use the
      Windows
      view in
      Device definition
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal