Device-defined data types (Generic ASCII)

Device-defined data type names vary for each serial protocol depending on the
Channel
selection in
Device definition
. These tables describe the device-defined data types created for the Generic ASCII protocol. The tables include information for input (as indicated by an "I") and information for output (as indicated by an "O").
Device-defined data type: AB:5000_ASCII:I:0
Name
Type
Definition
Valid Values
RunMode
BOOL
Channel operating state.
0 = Idle
1 = Run Mode
ConnectionFaulted
BOOL
Indicates if the connection is running. The device sets value to 0 when connected and then changes value to 1 when not connected.
0 = Connection running
1 = Connection is not running
DiagnosticActive
BOOL
Indicates if any diagnostics are active or if the prognostics threshold is reached.
0 = No diagnostics active
1 = One or more diagnostics are active or the prognostics threshold is reached
DiagnosticSequenceCount
SINT
Diagnostic counter. The value increments each time a distinct diagnostic condition is detected, and again when the condition transitions from detected to not detected.
Set to zero by product reset or power cycle. Wraps from 255 (-1) to 1 skipping 0.
-128 to +127
The value of 0 is skipped except during device power-up.
ASCII
AB:5000_ASCII_Channel:I:0
Channel array configurations.
Device-defined data type: AB:5000_ASCII_Channel:I:0
Name
Type
Definition
Valid Values
Fault
BOOL
Indicates that channel data is inaccurate and is not trusted for use in the application.
0 = Good
1 = Bad, causing fault
Tip:
If set to 1, troubleshoot the device to correct the cause of the inaccuracy.
Once the condition is removed, this is automatically reset to 0.
Uncertain
BOOL
Indicates that the channel data may be inaccurate, but the degree of inaccuracy is unknown.
0 = Good data
1 = Uncertain data
Tip:
If set to 1, troubleshoot the device to correct the cause of the inaccuracy.
Once the condition is removed, this is automatically reset to 0.
TxDataLost
BOOL
The transmitted data lost due to Transmit Buffer Overflow.
The bit remains set until Clear Buffer value changes from 0 to 1.
0 = Non-occurrence
1 = Occurrence
RxDataLost
BOOL
The received data lost due to Receive Buffer Overflow.
The bit remains set until Clear Buffer value changes from 0 to 1.
0 = Non-occurrence
1 = Occurrence
ParityError
BOOL
Indicates if a parity error occurred.
0 = Non-occurrence
1 = Occurrence
TxFIFOEmpty
BOOL
Indicates if data is in transmit FIFO.
The output FIFO has not sent all of its data to the ASCII device.
0 = Not Empty
1 = Empty
RxFIFOEmpty
BOOL
Indicates if data is in the receive FIFO.
The input FIFO did not send all of its data to the interface.
0 = Not Empty
1 = Empty
NonDelimitedRecord
BOOL
An input record is received and sent to the interface that was not triggered by receiving a delimiter character. This event occurs when either the buffer is filled to its maximum receive size or a Message Timeout has occurred.
0 = Not Produced
1 = Produced
HandshakeError
BOOL
Handshake error. Used for Handshake mode only.
0 = Non-occurrence
1 = Occurrence
NewData
BOOL
New data exists in the device. Used for Handshake mode only.
0 = None
1 = New Data
TxDataSent
BOOL
Indicates that the device sent data to serial port indicated by the Transmit Transaction ID and can accept more transmit data.
0 = Not Complete
1 = Complete
TxDataLengthInvalid
BOOL
Indicates if the TxDataLength is valid.
0 = Correct
1 = Length of TxDataLength is illegal
RxDataLengthInvalid
BOOL
Indicates if the RxDataLength is valid.
0 = Correct
1 = Length of RxDataLength is illegal
1
FramingError
BOOL
Indicates if a framing error occurred.
0 = Non-occurrence
1 = Occurrence
BufferOverRun
BOOL
Indicates if a buffer overrun occurred.
0 = Non-occurrence
1 = Occurrence
CTS
BOOL
Indicates if the CTS is active.
0 = Inactive
1 = Active
RTS
BOOL
Indicates if the RTS is active.
0 = Inactive
1 = Active
DSR
BOOL
Indicates if the DSR is active.
0 = Inactive
1 = Active
DCD
BOOL
Indicates if the DCD is active.
0 = Inactive
1 = Active
DTR
BOOL
Indicates if the DTR is active.
0 = Inactive
1 = Active
XOFF
BOOL
Indicates that the device stop sending data (Xoff) or not (Xon).
0 = On
1 = Off
BREAK
BOOL
Shows if a Break Interrupt occurred.
If a Break Interrupt is detected, the device keeps receiving binary data from the serial port.
The Receive data includes null Data (0x00).
0 = Not Detected
1 = Detected
TxACK
SINT
Feedback from the latest Transmit Transaction ID acknowledged by the serial device.
-128 to +127
RxID
SINT
Notification of receiving by updating number.
-128 to +127
RxDataLength
INT
Data length in RXData.
1 to 256
RxData
SINT[256]
Received data from modem.
-128 to +127
Device-defined data type: AB:5000_ASCII:I:1
Name
Type
Definition
Valid Values
RunMode
BOOL
Channel operating state.
0 = Idle
1 = Run Mode
ConnectionFaulted
BOOL
Indicates if the connection is running. The module sets this value to 0 when connected and then changes the value to 1 when not connected.
0 = Connection running
1 = Connection is not running
DiagnosticActive
BOOL
Indicates if any diagnostics are active or if the prognostics threshold is reached.
0 = No diagnostics active
1 = One or more diagnostics are active or the prognostics threshold is reached.
DiagnosticSequenceCount
SINT
Diagnostic counter. The value increments each time a distinct diagnostic condition is detected, and again when the condition transitions from detected to not detected.
Set to zero by product reset or power cycle. Wraps from 255 (-1) to 1 skipping 0.
-128 to +127
The value of 0 is skipped except during device power-up.
ASCII
AB:5000_ASCII_Channel:I:1
Generic ASCII produce data.
Device-defined data type: AB:5000_ASCII_Channel:I:1
Name
Type
Definition
Valid Values
Fault
BOOL
Indicates that channel data is inaccurate and is not trusted for use in the application.
0 = Good
1 = Bad, causing fault
Tip:
If set to 1, troubleshoot the device to correct the cause of the inaccuracy.
Once the condition is removed, this is automatically reset to 0.
Uncertain
BOOL
Indicates that the channel data may be inaccurate, but the degree of inaccuracy is unknown.
0 = Good data
1 = Uncertain data
Tip:
If set to 1, troubleshoot the device to correct the cause of the inaccuracy.
Once the condition is removed, this is automatically reset to 0.
TxDataLost
BOOL
The transmitted data lost due to Transmit Buffer Overflow.
The bit remains set until Clear Buffer value changes from 0 to 1.
0 = Non-occurrence
1 = Occurrence
RxDataLost
BOOL
The received data lost due to Receive Buffer Overflow.
The bit remains set until Clear Buffer value changes from 0 to 1.
0 = Non-occurrence
1 = Occurrence
ParityError
BOOL
Indicates if a parity error occurred.
0 = Non-occurrence
1 = Occurrence
TxFIFOEmpty
BOOL
Indicates data is in transmit FIFO.
The output FIFO did not send all of its data to the ASCII device.
0 = Not Empty
1 = Empty
RxFIFOEmpty
BOOL
Indicates data is in the receive FIFO.
The input FIFO did not send all of its data to the interface.
0 = Not Empty
1 = Empty
NonDelimitedRecord
BOOL
An input record is received and sent to the interface that was not triggered by receiving a delimiter character. This event occurs when either the buffer is filled to its maximum receive size or a Message Timeout has occurred.
0 = Not Produced
1 = Produced
HandshakeError
BOOL
Handshake error. Used for Handshake mode only.
0 = Non-occurrence
1 = Occurrence
NewData
BOOL
New data exists in the device. Used for Handshake mode only.
0 = None
1 = New Data
TxDataSent
BOOL
Indicates that the device sent data to serial port indicated by the Transmit Transaction ID and can accept more transmit data.
0 = Not Complete
1 = Complete
TxDataLengthInvalid
BOOL
Indicates if the TxDataLength is valid.
0 = Correct
1 = Length of TxDataLength is illegal
RxDataLengthInvalid
BOOL
Indicates if the RxDataLength is valid.
0 = Correct
1 = Length of RxDataLength is illegal
1
FramingError
BOOL
Indicates if a framing error occurred.
0 = Non-occurrence
1 = Occurrence
BufferOverrun
BOOL
Indicates if a buffer overrun occurred.
0 = Non-occurrence
1 = Occurrence
CTS
BOOL
Indicates if the CTS is active.
0 = Inactive
1 = Active
RTS
BOOL
Indicates if the RTS is active.
0 = Inactive
1 = Active
DSR
BOOL
Indicates if the DSR is active.
0 = Inactive
1 = Active
DCD
BOOL
Indicates if the DCD is active.
0 = Inactive
1 = Active
DTR
BOOL
Indicates if the DTR is active.
0 = Inactive
1 = Active
XOFF
BOOL
Indicates that the device stop sending data (Xoff) or not (Xon).
0 = On
1 = Off
BREAK
BOOL
Shows if a Break Interrupt occurred.
If a Break Interrupt is detected, the device keeps receiving binary data from the serial port.
The Receive data includes null Data (0x00).
0 = Not Detected
1 = Detected
TxACK
SINT
Feedback from the latest Transmit Transaction ID acknowledged by the serial device.
-128 to +127
RxID
SINT
Notification of receiving by updating number.
-128 to +127
RxDataLength
INT
Data length in the RXData.
1 to 256
RxData
SINT[256]
Received data from modem.
-128 to +127
Length is greater than the Max buffer length defined in
Device definition
.
Device-defined data type: AB:5000_ASCII:O:0
Name
Type
Definition
Valid Values
ASCII
AB:5000_ASCII_Channel:O:0
Channel array configurations.
Device-defined data type: AB:5000_ASCII_Channel:O:0
Name
Type
Definition
Valid Values
TxID
SINT
Transmit Transaction ID. Increment this value to transmit data from the serial port.
-128 to +127
RxID
SINT
Received Transaction ID. Increment this value to receive data from the serial port.
-128 to +127
TxDataLength
INT
Transmitted Data length of each channel.
1 to 255
ClearBuffer
BOOL
If Clear Buffer value changes from 0 to 1, the Receive and Transaction buffer is cleared.
0 = No Change
1 = Buffer Cleared
DTR
BOOL
DTR line signal level sent out when rising edge of EXEC bit is detected.
0 = Inactive
1 = Active
RTS
BOOL
RTS line Signal level sent out when rising edge of EXEC bit is detected.
0 = Inactive
1 = Active
EXEC
BOOL
If EXEC bit changes from 0 to 1, the device outputs a signal level which is set in the DTR/RTS tag.
0 = Inactive
1 = Active
RxDataLength
INT
Received Data length of each channel.
1 to 256
TxData
SINT[256]
Output data from the device.
-128 to +127
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal