Device-defined data types
The 5069-SERIAL device has two communication ports named
Channel 0
and Channel 1
. Each channel can be used as one of these serial protocols:- Generic ASCII
- Modbus Master
- Modbus Slave
The DF1 and DH485 protocols are applicable for Channel 1 and when a device is added under local chassis:
- DF1 Master
- DF1 Point to Point
- DF1 Radio Modem
- DF1 Slave
- DH485
Channel | Input Data Type | Output Data Type |
|---|---|---|
Generic ASCII | AB:5000_ASCII:I:0 | AB:5000_ASCII:O:0 |
Modbus Master | AB:5000_ModbusMaster_Status_<XXXXXXXX>:I:0 AB:5000_ModbusMaster_<XXXXXXXX>:I:0 | AB:5000_ModbusMaster_Run_<XXXXXXXX>:O:0 AB:5000_ModbusMaster_<XXXXXXXX>:O:0 |
Modbus Slave | AB:5000_ModbusSlave:I:0 | AB:5000_ModbusSlave:O:0 |
Channel | Input Data Type | Output Data Type |
|---|---|---|
Generic ASCII | AB:5000_ASCII:I:1 | AB:5000_ASCII:O:0 |
Modbus Master | AB:5000_ModbusMaster_Status_<XXXXXXXX>:I:1 AB:5000_ModbusMaster_<XXXXXXXX>:I:1 | AB:5000_ModbusMaster_Run_<XXXXXXXX>:O:1 AB:5000_ModbusMaster_<XXXXXXXX>:O:0 |
Modbus Slave | AB:5000_ModbusSlave:I:1 | AB:5000_ModbusSlave:O:1 |
DF1 Master | AB:5000_DF1_Master:I:0 | AB:5000_DF1_Master_P<n>N<m>:O:0 |
DF1 Point to Point | AB:5000_DF1_PointToPoint:I:0 | AB:5000_DF1_PointToPoint:O:0 |
DF1 Radio Modem | AB:5000_DF1:I:0 | AB:5000_DF1_RadioModem:O:0 |
DF1 Slave | AB:5000_DF1:I:0 | AB:5000_RunMode:O:0 |
DH485 | AB:5000_DF1:I:0 | AB:5000_RunMode:O:0 |
Provide Feedback