Channels view parameters (RTD devices)
Parameter | Description |
|---|---|
Channel | Indicates the channel to which the configuration applies. |
Sensor Type | Specifies the sensor type. Valid values are:
This parameter is not available in Run mode. |
Units | Specifies the temperature type. Valid values are:
This parameter is not available in Run mode and when
Sensor Type is set to
Ohms . |
Digital Filter | Specifies the desired filter time constant from 0 ms through 10000
ms. The default is 0 ms. This parameter is not available in Run mode. |
High Engineering Low Engineering | Displays the scaling high/low units based on the type of sensor. See the valid values in High/Low Engineering values (RTD devices). |
Notch Filter | Specifies the desired filter frequency for the device. Valid values are:
This parameter is not available in Run mode. |
Provide Feedback