Calibration Wizard parameters (output devices)
Parameter | Description |
|---|---|
Channel | Indicates the channel to which the configuration applies. |
Calibrate | Specifies the channels to calibrate. This parameter is not available in Run mode and Remote Run mode. |
Calibration Range | Indicates the calibration range. |
Calibration Status | Indicates the status of the calibration per channel as the
calibration occurs. Valid values include:
|
Low/High Reference | Indicates the calibration type.
|
Recorded Reference | Specifies the measured value in milliamps (mA) or Volts (V) in the
Calibration Range as shown in Low/High value. |
Status | Reveals the results of the calibration process as
OK or Error . |
Retry | Starts the calibration process over for the channels that did not
calibrate successfully. This parameter is available if the calibration process fails for one
or more channels. |
Provide Feedback