Calibration view parameters (RTD devices)

Parameter
Description
Channel
Indicates the channel to which the configuration applies.
Sensor Type
Indicates the sensor type as follows:
  • Ohms
  • 100 ohm Pt 385
    (default)
  • 200 ohm Pt 385
  • 100 ohm Pt 3916
  • 200 ohm Pt 3916
  • 10 ohm Cu 427
  • 120 ohm Ni 672
  • 100 ohm Ni 618
  • 120 ohm Ni 618
Calibration Range
Indicates the calibration range as follows:
  • 0 ohm to 64.9 ohms
  • 0 ohm to 250 ohms
  • 0 ohm to 500 ohms
    (default)
  • 0 ohm to 1000 ohms
The Calibration Range value changes based on the Sensor Type value. See their relationship in Calibration Range values (RTD devices).
Calibration Status
Indicates the status of the calibration per channel as the calibration occurs. Valid values include:
  • OK
  • Error
Start Calibration
Starts the calibration process while online.
This parameter is not available in Run mode and Remote Run mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal