Failed to schedule programs
Problem scheduling the program(s) on the
Schedule
tab of the Task Properties
dialog box.This may occur if the maximum number of scheduled programs is exceeded.
Cannot schedule more than 1000 programs to a single task. If this limit is exceeded, choose a different task to schedule this program, or remove one of the existing programs from the task.
Provide Feedback