Notification or error messages
List of notification or error messages encountered when working with tasks, programs, and routines in the Logix Designer application.
Message |
|---|
Failed to create the task (settings) |
Failed to create the task (name) |
Failed to create the task (values) |
Failed to create the task (initial combination) |
Failed to create the task (settings combination) |
Failed to schedule the program (combination) |
Provide Feedback