HMI navigation for PAID
Use the
HMI Navigation
tab on the PAID Properties
dialog box to enable or disable navigation from the HMI to process variable (PV) objects for Process Dual Sensor Analog Input (PAID) instructions.To enable HMI navigation to process variable objects for PAID instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
. - In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Under theHMItab, selectNavigation.
- To allow navigation to the PV A, PV B, and Output PV objects from the HMI faceplate, select theAllow navigationcheckboxes.
- In theObject tag namebox, enter the name of the object.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. Displays the current device status: PV good, PV uncertain, or PV bad.
- Device issues. Displays fault conditions: None, Fail, or Configuration error.
- SelectApply.
Provide Feedback