PAID input values and commands
Use the
General
tab on the Properties
dialog box for Process Dual Sensor Analog Input (PAID) instructions to monitor values for the process variable (PV) and two inputs, and to send online commands to select the PV value.To monitor input values and send online commands for PAID instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
. - In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Monitor the input values for the process variable, signal A, and signal B.TIP: Use theHMItab to add a label for signal A and signal B and a label that identifies the units for all three values.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. Displays the current device status: PV good, PV uncertain, or PV bad.
- Device issues. Displays fault conditions: None, Fail, or Configuration error.
- When online with the controller, use theseOnline commands.NOTE: The action is immediate if the command request does not need to be confirmed by the operator. If the command request requires a signature, this will enforce security from the HMI and disable commands and settings from the Logix Designer dialog.Online commandDescriptionMaximumSets the PV value to the higher of the two input values.MinimumSets the PV value to the lower of the two input values.A:Signal ASets the PV value to input A.AverageSets the PV value to the average of the two input values.B:Signal BSets the PV value to input B.
Provide Feedback