Review the decoration settings

The Library Content column displays all parameters, functions, and external references added to a library object in the
Library Designer
. All settings for decorative elements can be reviewed but not edited in the
Library Object Manager
application.
To review the decoration for a library object
  1. Select a library object in a folder or database repository. The
    Library Content
    column and
    Properties
    panel activate.
  2. Right-click the
    Definition Data
    listing and then select
    Expand All
    .
    The column displays listings for all parameters, functions, and external references added to the library object.
  3. Click a listing for a decorative element to review its settings in the
    Properties
    panel.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal