Add FT Historian content
FactoryTalk Historian
can be used to monitor tags on Logix objects. FactoryTalk Historian
collects time series data from process equipment, manufacturing devices, and other main data sources that are important to an operation.With this data when a specific event such as a downtime event, a bad batch, or an alarm occurs, process variables in the
FactoryTalk Historian
for the same time frame as the event can be reviewed and any correlations that might explain the event can be investigated and additional steps taken as needed to address any issues identified.Follow these steps to add
FactoryTalk Historian
content.- Right-click the library object in theLibrary Contentcolumn and selectAdd Section > FT Historian.AnFT Historianfolder, with the subfolderHistorian Tags, is added to the library object.
Provide Feedback