Add Attachments

How do I open Add Attachments?
  • In
    Library Content
    , right-click
    Attachments
    , and then select
    Add
    .
Use
Add Attachments
to add, edit, remove, import, or export file attachments to or from an
Application Code Manager
database.
Button or Column
Description
Add New Attachment
Opens
Attachment
to add an attachment file to the database.
Edit
Opens
Attachment
to edit the properties of an existing attachment file.
Extract Files
Extracts the selected attachment files to a folder location. The output files are extracted to their original filenames and formats.
Export to .HZ1 Attachment Files
Exports the selected attachment files to a folder location. The output files are exported with filenames matching the file ID in the .HZ1 format.
Import from .HZ1 Attachment Files
Imports one or more .HZ1 format attachment files from a folder location.
Filter
Limits the attachment list to attachments with properties matching the characters entered in the
Filter
field.
The filter function uses exact character matching and is case insensitive. Wildcard characters are not supported.
Select
Toggles whether a row is selected before deleting or exporting the attachments.
Name
Displays the name of the attachment.
Description
Displays the description of the attachment.
File Name
Displays the original file name of the attachment.
File ID
Displays the unique file identification number of the attachment.
Include Condition
Displays the Include Condition of the attachment. The default is Always. To create an Expression, click the ellipsis (...) button to open the
Expression Builder
. Double-click the selected attachment to open
Attachment
, and then you can configure the attachment. A condition can be entered manually or generated by an expression.
Extraction Path
Displays the extraction path of the attachment. To create an Expression, click the ellipsis (...) button to open the
Expression Builder
. Double-click the selected attachment to open
Attachment
, and then you can configure the attachment. A path can be entered manually or generated by an expression.
Revision Description
Displays the latest revision description of the attachment.
Modified Date
Displays the last modified date of the attachment.
Modified By
Displays the last user that modified the attachment.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal