Change the include condition

Change the include condition of an attachment reference to determine when
Application Code Manager
extracts and publishes the attachment from the project. The attachment is only extracted if the include condition evaluates to true.
To change the include condition of an attachment reference
  1. In
    Library Object Manager
    , from
    Library Repositories
    , select a library.
  2. In
    Library Content
    , expand
    Attachments
    , then select an attachment reference from the list.
  3. In the properties pane, select the ellipsis button
    (...)
    next to
    Include Condition
    to open Expression Builder.
  4. In
    Expression Builder
    , modify, test, and save the include condition, then select
    OK
    .
  5. Click
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal