Copy a DDE Link to the clipboard from the data monitor

  1. From the data table display, select the data element you want to copy.
  2. Right-click and select
    Copy to Clipboard
    . Copying the DDE link to the clipboard may initiate the Topic Configuration or Copy Link to Clipboard dialog box. Refer to the help associated with these dialog boxes for more information.
  3. For simple DDE transfers, click
    OK
    or
    Done
    to select the defaults.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal