Create a Next Pen button
Use the Next Pen button object with the trend object. Pressing the button switches the trend to the next pen’s y-axis.
To create a Next Pen button
- In theGraphic Displayeditor, selectObject > Trending > Next Penor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify the options as needed.
Provide Feedback