Create a Pause Pen button
Use the
Pause Pen
button object to toggle the selected trend chart between pausing and resuming automatic scrolling.To create a Pause Pen button
- In theGraphics Displayeditor, selectObject > Trend > Pause Buttonor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify the options as needed.
Provide Feedback