View alarms and messages at runtime
The operator can view alarms and other messages at runtime using these graphic objects and graphic displays:
This information | Appears in this object | In this default graphic display |
|---|---|---|
Alarm messages | alarm list | [ALARM] Alarm list |
System activity | diagnostics list | [DIAGNOSTICS] How the diagnostics list works at runtime |
Information messages | information message display | [INFORMATION] How the information message display works at runtime |
Local messages | local message display | no default display How the local message display works at runtime |
TIP:
The default alarm, information, and local message displays open automatically when the assigned tags match the messages’ trigger values. They can also be opened using goto display buttons. Operators can acknowledge and clear messages on these displays.
All of these objects can be placed on any graphic display.
Provide Feedback