Enter numeric and string values at runtime
The operator can enter values at runtime using these graphic objects:
To enter | Press this button object | Then enter values in the pop-up that opens |
|---|---|---|
Numeric values | Numeric input enable button Numeric input cursor point | Use the numeric pop-up keypad Use the numeric pop-up scratchpad How the numeric pop-ups work at runtime |
String values | String input enable button | Use the string pop-up keyboard Use the string pop-up character input Use the string pop-up scratchpad How the string pop-up keyboard works at runtime How the string pop-up scratchpad works at runtime |
Provide Feedback