Set up recipe properties for a RecipePlus table
Use the
Recipe
tab of the RecipePlus Table Properties
dialog box to set up recipe properties for the object.To specify what columns will be shown and how they will appear
- In theGraphics Displayeditor, double-click the recipe selector to open itsPropertiesdialog box.
- Click theRecipestab.
- Select and define the table's columns.
- Specify whether a header and/or footer will be shown.
- Specify whether the table will accept user input or will be view-only.
Provide Feedback