Create a RecipePlus table
The RecipePlus table object lists the ingredients in the recipe file most recently selected in the RecipePlus selector and restored. It can also be used to edit the data values for ingredients and to save those edited values to the recipe file.
The table displays:
- The name of each ingredient in the recipe (Ingredient namecolumn)
- The current value of each ingredient in the tag associated with the ingredient (Current valuecolumn)
- The data value assigned to each ingredient (Recipe valuecolumn)
- An X if the ingredient value is different than the tag value when the restore occurred (Compare statuscolumn)
- The tag name associated with each ingredient (Tag namecolumn)
- The recipe file name, the recipe unit name, the number of visible ingredients and the total number of ingredients (status bar at the bottom)
To create a RecipePlus table
- In theGraphics Displayeditor, selectObjects > RecipePlus > Tableor drag
from the toolbox. - Drag the mouse to position and draw a rectangle of the general size and in the general location that you want the table to be.
- Double-click the table to open itsPropertiesdialog box.
- In thePropertiestabs, specify how the table looks, how it will show recipes, and its common properties.TIP:There can only be one RecipePlus table on a graphic display. Attempts to add a second one produce an error message.
Provide Feedback