Create a polyline object
Use the polyline tool to draw a series of connected straight lines.
To create a polyline object
- In theGraphics Displayeditor, selectObjects > Drawing > Polylineor drag
from the toolbox. - Press the mouse button and drag the mouse to draw the first line segment.TIP:PressCtrlas you drag or click the mouse to draw a horizontal or vertical line segment.
- To create the next line segment, point the mouse where you want the next segment to end, and then click theLeft mousebutton.Repeat for each line segment.
- Double-click the polyline to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how you want the polyline to look.TIP:
- If you use the polyline tool to create an object with two points, it will create a line object.
- If you edit a polyline object by deleting its points until it has two points, it will convert to a line object.
Provide Feedback