Create a line object
Use the line tool to draw straight diagonal, horizontal, and vertical lines.
To create a line object
- In theGraphics Displayeditor, selectObjects > Drawing > Lineor drag
from the toolbox. - Press the mouse button and drag the mouse to draw a line.TIP:PressCtrlas you drag the mouse to draw a horizontal or vertical line.
- Double-click the line to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how you want the line to look.
- ClickOK.TIP:When you put a line intoEditmode and add a point to it, it is converted into a polyline object. If you remove a point from a polyline with three points, it becomes a line object.
Provide Feedback