Create a polygon object
Use the polygon tool to draw a series of connected straight lines forming a closed shape.
To create a polygon object
- In theGraphics Displayeditor, selectObjects > Drawing > Polygonor drag
from the toolbox. - Press the Mouse button and drag the mouse to draw the first line segment.TIP:PressCtrlas you drag or click the mouse to draw a horizontal or vertical line segment.
- To create the next line segment, point the mouse where you want the next segment to end, and then click the Left mouse button.The application automatically connects the last segment to the first. Keep clicking to add more line segments.
- Double-click the polygon to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how you want the polygon to look.TIP:
- Squares and rectangles are classified as specialized forms of polygons, but you use the rectangle tool to create them.
- Creating a polygon with only two points actually creates a line.
Provide Feedback